DOUT.STATES

Description

DOUT.STATES reads the states of the digital outputs. Each bit corresponds to a digital state. Bit 0 = DOUT1 ... Bit 8 = DOUT9.

Examples

Usage

When DOUT1 and DOUT3 are active (DOUT#.STATE = 1). Bits 0 and 2 would be set. DOUT.STATES would be 5.

Code

--> DOUT.STATES
5

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units N/A
Range 0 to 511
Default Value N/A
Data Type Integer
See Also  

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DOUT.STATES

3600h

00h

Unsigned32

-

-

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DOUT.STATES

2702

A8E

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DOUT.STATES

2702

Unsigned32

Read Only

-